MITSUBISHI ELECTRIC endringer til det bedre
Norway

Devices and Components

Networks

CC-Link Safety is an open communications network that is suitable for safety applications because it guarantees reliability in data transmission. It complies with IEC61508 SIL3 and EN954-1/ISO13849-1 Category 4 and is compatible with other CC-Link products. CC-Link Safety will detect communication failures such as unexpected delay of communication or erroneous data that may cause malfunction of the emergency stop operation. This fail-safe function will bring machinery into a safe condition quickly if a communication failure is detected.

Sensors

Mitsubishi Electric has a best in class strategy with regard to safety sensors that allows customers to select the products that optimize their application. From selecting e-stops to light curtains, Mitsubishi Electric provides the interfaces that enable connectivity to a broad range of safety sensor technologies.